Hello there,
I am using TPS259807ONRGER to monitor and switch off 12V and 5V rails when there is a short circuit.
My scenario is as follows:
When there is a short circuit the eFuse will shut off the power and then retry to turn on after 5seconds
During this 5seconds the PG signal will go low and trigger a buzzer.
After 5seconds pass, eFuse will try again and if there is no short circuit the buzzer will be off.
12V rail works as expected, but 5V rail do not perform the 5second delay.
I checked the RETRY_DLY pin, there is 90ms second period oscillation for the 12V rail.
But there is only DC on this pin for the 5V rail.
After repeatedly shorting 5V rail, the oscillations sometimes appear in that pin and therefore I have 5second delay.
Am I missing something or for 5V the oscillation does not start and/or unstable.
I will be greatful if you could help me.
Kind regards