This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51604: Selecting MOSFET driver for BOOST DC/DC converter

Part Number: TPS51604
Other Parts Discussed in Thread: LM5122, TIDM-BUCKBOOST-BIDIR, UCC27211

I'm working on project of StepUp DC/DC converter (12V to 24V, 200W, variable output voltage)

I'm looking for correct driver for MOSFET bridge.

Previously I used integrated mosfet bridge and  driver CSD97396 but unfortunately, (what was posted on this forum)  it didn't work correctly and generaly it can't work in BOOST application.

Next I found separate driver like TPS51604. It meet my requirements (like ability to direct control from 3.3V uC). But it again was designed to work in BUCK applikation.

So I would like to ask about sugestion to  driver that could work in BOOST converter stage. I'm  looking for driver and mosfet bridge component only because I plan to control this converter from microcontroller not dedicated complete controller like LM5122 because output voltage must be controled dynamically.
 

I will be gratefull for any help.