Hi,
Could you please advise what configuration is suggested to implement the Battery remote sense for BQ25306?
VIN 9-17V
BAT=2S1P Li-Ion
VBAT_max=8.4V
Ich=2.5A
The battery pack is connected to a 1-meter cable, which has a typical impedance of 50-70 mΩ for both the B+ and B- wires.
However, the specifications do not provide any information on how to implement the pack remote sensing.
Can you please advise which option would be preferable to implementing the battery remote sense?
Option1:
Option2:
Can we compensate for the voltage drop on the B-wire with a remote pack connection with BQ25306?
Regards
Vitaliy