Hi
We are using the LM5045 in one of our projects, with an output power of about 2kW. The converter operates across a wide output range, including CC or CV operations at 0-100%.
The issue we are encountering is instability and oscillation at light loads (low impedance load for CC operation). We have verified the stability of the PFC section, and the bulk voltage remains very stable. Loop analysis for the DC-DC side shows good gain and phase margins (>10dB for Gain and >60 deg for Phase) until the output becomes unstable.
Is there anything specific we should consider for this light load condition (less than 10% of full load)?
Any assistance would be appreciated. Thank you.