Dear Team,
Does TLV61220 can work at operating temperatures of -51 degrees?
If not, do you suggest us suitable solution? Thanks a lot.
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
TLV61220 can only support -40 degrees. Currently there is no such device that can support the EC table spec under -40 degrees. Can I ask what is the application , is the -51℃ typical ambient temperature?