Dear TI experts,
I have used your company's BQ76952 and encountered some issues.
1. When the LD pin is connected to the PACK through resistors (As shown in the following image), the discharge MOS is not initially turned on, and the PACK+ is suspended. So, how does BQ76952 open the discharge MOS through the DSG pin?
2. I have learned that during the discharge MOS shutdown process, the voltage of the DSG pin will follow the changes of the LD pin. But, what is the role of the LD pin during the charging process? And if I ground the LD pin, how does the DSG pin turn on the discharge MOS?
When I quickly clicked on the power switch on the circuit board, I found that the PACK+ terminal had an output when the discharge MOS was not turned on. Therefore, I would like to know if this is related to the internal structure of AFE BQ76952.
Thanks!