This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75469: Check the Vi(on) on p.5 of the SN75469 data sheet.

Part Number: SN75469
Other Parts Discussed in Thread: ULN2004A,

I answered the following question in the previous question, but is this answer correct?

A customer has contacted us to confirm.

The numbers are:

IC = 125mA --> 5V

IC = 200mA --> 6V

IC = 275mA --> 7V

IC = 350mA --> 8V

Best regards.