This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: BMS for Drone with 6S and 30A nominal

Part Number: BQ40Z80

Hello,
We are working on designing a BMS to manage the charging and discharging of a 6S battery. The BMS is intended to be incorporated into a drone, so it needs to have the smallest possible weight and size. The idea is to be able to charge the batteries without removing them from the drone and without turning it off. Initially, the charging current will be approximately 4A, and the discharge current can peak at 60A with a nominal current of around 30A.
In a preliminary review, we have decided to use the BQ40Z80, but we would like to know if there is another component more suitable for our purpose.

Attached is the schematic designed for the BW40Z80 component

Thank you very much for the help!

José Barroso

Schematic BQ40Z80.pdf