Part Number: BQ25708
Other Parts Discussed in Thread: BQ25700A, , BQ25756
Hi,
A related question recommends replacing BQ25700A with BQ25708. When replacing the BQ25708, the pin arrangement is the same except for the 5 pin of the NC, so will it be possible to operate by simply replacing the board without revising the board? Also, the data sheet says BAT temp thermistor monitoring, but could you tell me which terminal can be used for monitoring?
The functions required of a charging IC are as follows.
・Battery temperature monitoring possible
・Temperature management of charging IC
・Charging voltage: 8.25V
・Battery to be charged: Lithium ion battery (2cell)
As a background for the above question, we are considering evaluating the BQ25708 on EVM, but if there is a charging IC other than the BQ25708 that is suitable for the conditions, I would like to know.
Thanks,
Conor