This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546D24AEVM: TPS546D24AEVM

Part Number: TPS546D24AEVM


I understand the process of converting TPS546D24AEVM from 2 phase to single phase.

What changes has to be made to the output decoupling capacitors and the compensation circuitry with respect to 1 phase vs 2phase.

  •  

    There are no required changes to the output decoupling capacitors or the compensation to convert from 2-phases to 1-phase.  The 2-phase output has sufficient output capacitance to stablize the 1-phase loop.

    To fully utilize the available output capacitance, you can select a compensation code with 2x higher VLOOP due to the reduced current loop gain from the loss of 1-phase.

    This will provide similar transient performance to the original 2-phase design for the same load step, compensating for the reduced forward transconductance with increased voltage loop gain.

    The base EVM uses MSEL1 to AGND = 12.1kΩ (Resistor to Ground code 5) with no resistor to BP1V5 (Divider Code None).  Table 7-9 shows this selects Compensation Code 13 with ILOOP = 4 and VLOOP = 2.  Changing to Compensation Code 14 (ILOOP = 4, VLOOP = 4) is resistor to ground code 6 with no divider.  Table 7-17 shows this is a 14.7kΩ resistor to AGND (R21_P1)

    Alternately, you can remove 1/2 of the output capacitors.

    This will provide similar transient performance to the original 2-phase design for 1/2 the load step, leveraging the reduce forward transconductance to allow less output capacitance.

    If removing capacitors, I would recommend removing the capacitors furthest from L1, working closer to L1 to provide the loop with the least parasitic inductance possible after removing the capacitors.

  • Peter,

    Thanks for the detailed reply, I shall increase the Vloop to 2x to get a fair comparison between 1 and 2 phase implementation.