Other Parts Discussed in Thread: TPS25814, TPS65988
Hello,
I am currently developing the design for a USB dock that incorporates three ports. One port will serve for charging an Android tablet, the second port will be designated for a USB camera, and the third port will function as a USB power input to supply power to the system. The USB camera will draw power from the tablet/USB dock. I want to simultaneously transfer data to the tablet, allowing for tablet charging during data transfer.
To achieve this, I plan to employ the TPS25814 IC and have consulted the TPS25814EVM for reference. According to the above block diagram, the tablet must be linked to the DFP port for charging, while the UFP port will be connected to the USB camera, requiring a power supply. It's worth noting that in this configuration, there is no VBUS connection at the UFP port. I require assistance in resolving this matter. Would it be advisable to directly connect or short the VBUS between the UFP and DFP?