This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25125: Looking for a better part ?

Part Number: BQ25125


Hello,

I am using the BQ25125 to power a radio from a single cell at 3.3 volts.

Sadly, when I increase the output voltage from the 1.8 volts to 3.3 volts - the I2C quits working because

the thresholds are determined from Vsys - (not clear in the datasheet).

In my all 1.8 volt design - this will require me to add a level shifter.

Is there another part that has the DC-DC and I2C that will work without a level shifter ?