Other Parts Discussed in Thread: LMR54406, LMQ66410
Hello Team
I'd like to concfirm validity of inductor selection design.
Our circuit requirement
Vin : 19V
Vout : 5.15V
Iout : 150mA (max)
I calculated inductor inductance constant with eq.(7) in the datasheet (Revision A Dec, 2022)
Do the parameters using calculation follow design guidline?
VIN=19V, VOUT=5.15V, Fsw=1.055MHz, K by Iout_max = 0.2
Then, calculation result is 17.8uH
Also, are there any design guidelines for the current flowing into the Swichng Coil immediately after power on?
*VIN and EN are used short-circuited.
Best Regard
Miyano Shinichi