Part Number: TPS65219
Other Parts Discussed in Thread: AM2431, LP8733, ,
Hi Experts,
We are in a board design with AM2431 MCU along with LPDDR4 and 2 No.s of RGMII Ethernet. (Voltage rails are 0.85V, 1.1V, 1.8V, 2.5V & 3.3V).
I am planning to use a power supply solution either with LP8733 or with TPS65219.
My doubt here is about the PMIC programming.
In order to use the above PMICs with AM2431, do we need to program the PMICs from our end ?
Or , The PMICs NVM will be coming with a default program in it? so that we can directly use the parts in our board.
Please suggest.
Regards,
Salman