Hello Team
I am Developing Isolated DC to DC using LM5156 for below specification.
Industrial Application
Input voltage-16 to 40VDC
Output volate-5V
Output current- 3.5A
1.How should I add Latch protection in the same Circuit?
Latch protection -In case of any faults, System will re-start Only after input power is switched off and On
2. Or is there any PWM IC available with latch mode for above specification.
Thanks
Aditya