Hi team,
My customer is using our UCC27201A. They use MPPT voltage as flyback's input, flyback output 12V to power the UCC27201A. The UCC27201A part sch as below:
They find sometime when the MPPT input is above 50V, our UCC27201A will be damaged and output abnormal as below:
(CH1:High side MOS Vgs;CH2:5Pin(HI);CH3:6Pin(LI);CH4:Low side MOS Vgs)
I have asked them to check if the 12V input stable when MPPT is 50V since the max VDD is 20V.
Could you please also help check why the output is abnormal and if there's any other thing need customer to check to find the root cause of the device damage?
Thanks,
Brian