This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Battery Disconnect / BQ Reset Detection

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ34Z100-R2, BQ34Z100, GPCCHEM, EV2400, BQSTUDIO, BQ34Z100EVM, BQ40Z50

Hello,

I have a fleet of devices using the BQ34, and I suspect we are having battery issues because we detect a reset on our microcontrollers, and the BQ's coulomb counter almost seems to be reset because after the real SOC of 20% shoots up to the incorrect SOC of 100%. For the next 24 hours, the BQ will report a declining SOC of 100 -> 92%, and at the exact 24-hour mark, it shoots back down to ~20% as expected and stays there.

Are there any registers that I could use to detect that a power cycle of the whole device has occurred? I am assuming that the non-persistent algorithm used to determine SOC is being cleared, which causes a really rough estimate for the next 24 hours. To detect a reset, checking things like charge cycles or discharge cycles doesn't feel very reliable. Also, I thought maybe the CF flag would help, but it doesn't seem to change when I power cycle my desk device.

Thanks,

AJ