Part Number: TPS25730
Other Parts Discussed in Thread: TPS3701, SM74611,
Hi,
I want to add USB PD to an existing 24V device. Users can either select a barrel jack or USB type-C. A 20V/3A profile is chosen by resistor values.
What happens when a user is connected via USB type-C (Power path conducting, enabled) and the 24V barrel jack is inserted and applied to PPHV?
- Will the overvoltage protection kick?
- Will the reverse current protection kick in?
If they don't, then I need to close/disable the conducting path by asserting FAULT_IN low with the help of a lot of external components (TPS3701, TIDUAZ2).
Or use a diode or ideal diode (SM74611) to prevent back feed onto Vbus.
The datasheet only mentions Vbus overvoltage situations and not Vpphv overvoltage situations.