Other Parts Discussed in Thread: TPS7A69-Q1,
Hi, Team,
What is the spec difference between TPS7A6933-Q1 and TPS7B8533-Q1? Why is the price of x6933 is times of higher than x8533? Is x6933 not our hero device any more?
Thanks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Team,
What is the spec difference between TPS7A6933-Q1 and TPS7B8533-Q1? Why is the price of x6933 is times of higher than x8533? Is x6933 not our hero device any more?
Thanks~
Keely,
Please see spec difference. What are the volumes here, pricing is based on several factors and the difference here is due to performance, package and technology.
| TPS7A69-Q1 | TPS7B85-Q1 | |
| Iout(Max)(A) | 0.15 | 0.15 |
| Vin(Max)(V) | 40 | 40 |
| Vin(Min)(V) | 4 | 3 |
| Vout(Max)(V) | 5 | 5 |
| Vout(Min)(V) | 3.3 | 3.3 |
| Fixed output options(V) | 3.3, 5 | 3.3, 5 |
| PSRR @ 100 KHz(dB) |
40 | 70 |
| Noise(uVrms) | --- | 280 |
| Accuracy(%) | 2 | 1.5 |
| Dropout voltage (Vdo)(Typ)(mV) |
300 | 100 |
| Iq(Typ) (mA) |
0.012 | 0.02 |
| Output capacitor type | Ceramic | --- |
| Thermal resistance θJA(°C/W) |
113 | 47 |
| Operating temperature range(C) |
-40 to 125 | -40 to 150 |
| Package size: mm2 | 19 mm2: 3.91 x 4.9 (SOIC|8) | 9 mm2: 3 x 3 (VSON|10) |
| Packages | SOIC|8 |
VSON|10 |
Thanks,
Prakash L