Part Number: LM5146

What is the ideal way to drive the SYNCIN input from an external source?
Should this source be present and stable before the supply is enabled, after? Or is it inconsequential?
Should the 20K pull up to VCC be removed when using an external sync clock?
In the attached schematic, using the LTC6908IS6-1 to generate the sync input w/ the 20k pull up present, and 5V source turning on after the 3.3V supply, it causes the 3.3V supply to be unstable and not recover, until powered off and the frequency removed from SyncIN by depopulating R419.


Blue is 3.3V, Red SYNCIN.