Other Parts Discussed in Thread: LP5813, , LP5812
Hello,
I'm looking to evaluate the LP5813 with board LP5813-12WCSPEVM. The data sheet mentions the LP581xGUI software.
Is there a download link available?
Regards,
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm looking to evaluate the LP5813 with board LP5813-12WCSPEVM. The data sheet mentions the LP581xGUI software.
Is there a download link available?
Regards,
Kevin
Hi Kevin,
Please refer the below link to download the GUI first, the formal GUI hasn't been released on ti.com.
Link: tidrive.ext.ti.com/.../bc48b442-7bb4-4ca9-8817-37bb0bc3791c
Access code: XeTc59.N
Please free to contact me if there is any questions.
BR, Jared
Hi Jared,
Do you know when it will be released? The EVM arrived this morning and cannot get the link to work (auth fail).
Hi Cameron,
I am not sure when the formal GUI will be released. Please use the internal GUI first, here is the update link:
Link: https://tidrive.ext.ti.com/u/oNE-O1hRPj6y0T4o/bc48b442-7bb4-4ca9-8817-37bb0bc3791c?l
Access code: 84zpwE(Y
BR, Jared
Hi Van,
Please find the updated GUI link below:
Link: tidrive.ext.ti.com/.../bc48b442-7bb4-4ca9-8817-37bb0bc3791c
Access code: Nk{8JF6d
BR, Jared
Hi Eric,
Sorry to late reply. Since the official GUI still has some problems during testing, it has caused a slight delay. Sorry for the inconvenience.
BR, Jared
Thanks Jared, software has a few issues yet, so I am controlling the LP5812 from our target PCB directly. When I send the register settings from the programming example in the data sheet 9.2.3.3, only D1 and D2 illuminate. Jumper settings on the EVM are the same as figure 2.5 in the EVM guide (except for the I2C jumpers that are set for external power and no additional pull-ups. The scope shows what i believe to be the correct signals/levels for 4 scan TCM on all diode pins. Also setting register 0x44 to a positive value does not illuminate the green led of D1. Does it sound like D3 and D4 have failed, or is there some register setting missing form the programming example?
Hi Van,
Could you please send me a email (jared-zhou@ti.com) for detail discuss?
BR, Jared
Hi Jared, I'm also looking for the GUI if you could please provide an updated download link.
Hi Tyler,
Could you please send me a email (jared-zhou@ti.com) and I will forward the LP581x GUI to you? Thanks!
BR, Jared
Hi Gerald,
Could you please send me a email (jared-zhou@ti.com) and I will forward the LP581x GUI to you? Thanks!
BR, Jared
Hi Vladimir,
Same answer - Could you please send me a email (jared-zhou@ti.com) and I will forward the LP581x GUI to you? Thanks!
BR, Jared