HI ti team
I am having a problem using BQ25798.When I set FORCE_IBATDIS=1, how do I check to see if it is running? Will BQ25798 enter HIZ mode when VBAT pin is detected no battery?If my battery takes about 3s to wake up and I enable the FORCE_IBATDIS function, will it fail to charge due to a false detection of no battery