Hello dear, I want to enquire about the induction selection in section 8.2.2.1 of page 18 of the datasheet. What is the maximum input power averaged over the ac line period in this case? And how can you calculate/determine it?
Kind regards
Bright
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello dear, I want to enquire about the induction selection in section 8.2.2.1 of page 18 of the datasheet. What is the maximum input power averaged over the ac line period in this case? And how can you calculate/determine it?
Kind regards
Bright
Hello,
Section 8.2.1 gives design specifications for the applications.
This design has an efficiency target at max load of 0.9.
With this information you can calculate Pin as follows.
Pin = Pout/efficiency = 100 W/0.9 = 111.11 W
Regards,
Hello Mike,
Thanks for your switch response.
Regarding calculating the inductor value on 8.2.2.1 inductor selection, what is the switching frequency that should be used in the example. I understand that the switching frequency is determined automatically based on the mode of operation, for example CCM, DCM as mentioned in section 7.4.1. In this sense, how do you select the switching frequency to use to calculate for inductor selection on section 8.2.2.1.
Kind regards,
Bright
Hello Mike,
Thanks for your switch response.
Regarding calculating the inductor value on 8.2.2.1 inductor selection, what is the switching frequency that should be used in the example. I understand that the switching frequency is determined automatically based on the mode of operation, for example CCM, DCM as mentioned in section 7.4.1. In this sense, how do you select the switching frequency to use to calculate for inductor selection on section 8.2.2.1.
Do I need to use the minimum Switching Frequency of 5kHz?
Kind regards,
Bright