This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21220: Comply with IEC 60950-1 and IEC 62368-1?

Part Number: UCC21220


Hi Team,

My customer needs to meet IEC 60950-1 and IEC 62368-1 on their end equipment, could UCC21220 & UCC21220A comply with these 2 certifications?

BTW, may I confirm the progress on DIN EN 61010-1 and GB4943.1-2011? The status still shows "planned" in the datasheet.

Regards,

Charles 

  • Hi Charles, 

    Update: IEC60950-1 and IEC62368-1 are system standards, and UCC21220 can be used in system design to meet those standards. May I ask what customer and EE you're working with? 

    Regarding the certification, we do have VDE and CQC completed. The latest CQC standard is GB 4943.1-2022 and the latest VDE standard is DIN EN IEC 60747-17, and UCC21220 is certified for both. 

    Thanks! 

    Vivian