Other Parts Discussed in Thread: TPS25751
Dear sir,
While looking for a USB-PD Extended Power Range (EPR) bidirectional converter 10S lithium battery charging solution, I stumbled upon TI’s “BQ25756” solution. I have some questions about this:
1. The input voltage range is shown as 5V / 9V by , the output voltage is 30-42V, and the charging current is 650mA. Is 27W suitable for this IC design?
2. The input voltage range is shown as 5 to 15V, the output voltage is 30-42V, and the charging current is 250mA. Is 12W suitable for this IC design?
3. Study 2. ICHG_REG register bits (host software control), describe "To set the maximum charge current using the ICHG_REG register bits, write to the ICHG_REG register bits.
The charge current limit range is from 400 mA to 20,000 mA with 50 mA/step. The default ICHG_REG is set to
maximum code, allowing ICHG pin to limit the current in hardware"
In 8.3.4.1.1 Charge Current Programming (ICHG pin and ICHG_REG)), page 24 of data sheet.
The minimum charging current is limited to 400mA? How to set it to 250mA?
Best Regards,
Giedi Wang