This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power design solution recommendations

Guru 12655 points

Other Parts Discussed in Thread: LM5155, LM5156

Hello,

My client is looking for solutions that can be designed to meet the following conditions:

   - Input voltage: 4V ~ 60V
   - Output power:50W
   - Output Voltage: 5V or 12V

Q1. Is there a device or module that can support the above conditions as an isolation type?

Q2. Is there a device or module that can support the above conditions as an non-isolation type?

Q3. If you have an appropriate design reference for the above conditions, please provide it.

Thank you.

JH