Hello Team
I am designing Isolated DC to DC converter using LM5156 for below Specification.
Input - 17 to 32 VDC
Output - 5V
Output Current: 3.5A
I need solution for below Condition.
Condition: When my input voltage is below 16VDC at that time My controller needs to turn off and I want to achieve Output voltage hold on for 10ms.
for this condition any calculation available?
Please suggest how should I achieve.
Thanks
Aditya