Hi, I have the same problem regarding the use of the unencrypted LM5117 model. I've used it in microcap and gave the same error about the T (0,0) and when deleting it a singularity error occurs. Therefore, I implement it on the LTspice and it gave me an error of V3 has been shorted (V3 been a variable inside the LM5117 coding) when trying to simulate. My question would be if the problem is in the code, or it might be a bad connection made outside the model? In any of the two cases, what should I do to solve the problem? Thank you in advance.