Part Number: UCC28740
Other Parts Discussed in Thread: TL431
Hi,
I designed a flyback converter with UCC28740 using WEBENCH tool and datasheet. My converter operated well, when i connect 200V from input, i can get 5V from output. But when i load the converter, while I should be able to load the circuit up to 2A, I can load it up to a maximum of 200mA and then the circuit turns itself off. Moreover, from the moment I connect the load, even the slightest increase in the load causes the output voltage to decrease rapidly. What could be the reason for this? My circuit design image is below.
Thank you.
Transformer spec- Np;Naux;Ns = 152;20;6 , Lp=2.56mH
I also tried to change Rcs and using respectively 2.1 - 5.1 - 10ohm but it didnt change anything.