This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM8D6B24: Support in Fusion Digital Power Designer

Part Number: TPSM8D6B24
Other Parts Discussed in Thread: TPSM8D6C24, TPSM846C23, TPS546D24A

In this 1 year old thread the question, if there will be support for the TPSM8D6B24 in the Fusion Digital Power Designer, was already answered:

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1160247/tpsm8d6b24-fusion-digital-power-designer

The device should have been added by last year to the "Fusion GUI Power Designer", which is a software I could not find anywhere. Instead I am now using the Fusion Digital Power Designer v7.10.1 [2023-10-27] and I can not select the TPSM8D6B24. Am I using the wrong software? Can you provide a link to the correct software? Or is there some add-on, that I need to install?

Best regards and thank you!

  • Hello,

    The Fusion Digital Power Designer and the "Fusion GUI" are the same tool, so you are using the right software! Are you using Fusion in offline mode? If so, you can select the TPSM8D6C24 from the list of available devices. These devices share the same user interface and command list. I will confirm on my side that TPSM8D6B24 can be detected on a live device, it will take me a few days to receive the evaluation board & confirm. I will update you here

    Best regards,

    Britton

  • Dear Britton,

    Thank you for your fast reply. I had a look in the Fusion offline mode, however, I can only find the following device list:

    Offline Device List

    The only module that can be found is the TPSM846C23, which has only one rail and therefore seems to differ from the TPSM8D6C/B24 that I should be looking for.

    When it comes to the online mode, I can verify the device responding to a Raspberry Pi I2C scan and the USB Interface Adapter is recognized by the software. So I seem to be only lacking the device in the list.

    Thank you and best regards,

    Torben

  • Hi Torben,

    The TPSM8D6C24/B24 actually use the same command list and user interface as TPS546D24A.  Feel free to select TPS546D24A from the offline list or you can open the attached file below, which is a system file pulled directly from a TPSM8D6C24 evaluation board. Please refer to the steps below for opening the system file:

    1. Download the system file for TPSM8D6C24

     

    <?xml version="1.0" encoding="utf-8"?>
    <ProjectData xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns:xsd="http://www.w3.org/2001/XMLSchema">
      <Version>1</Version>
      <Timestamp>2023-12-20T10:06:46.7995282-06:00</Timestamp>
      <Creator>Texas Instruments Fusion Digital Power Designer v7.9.3.0.Beta [2023-03-31]</Creator>
      <Devices>
        <Device>
          <PartID>TPSM8D6C24</PartID>
          <Address>20</Address>
          <Is_Offline>false</Is_Offline>
          <SAA_Number>1</SAA_Number>
          <Saved_In_Offline_Mode xsi:nil="true" />
          <Saved_While_NVM_Write_Pending xsi:nil="true" />
          <Write_Protected>false</Write_Protected>
          <Package>0</Package>
          <Num_Outputs>1</Num_Outputs>
          <Parameters>
            <Parameter>
              <ID>VOUT_MODE</ID>
              <Code>32</Code>
              <IDAndCode>VOUT_MODE [0x20]</IDAndCode>
              <ValueText>Relative; EXP =-9</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x97" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>CAPABILITY</ID>
              <Code>25</Code>
              <IDAndCode>CAPABILITY [0x19]</IDAndCode>
              <ValueText>Max Bus: 1000 Khz; PEC: Yes; SMBALERT#: Yes</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0xD0" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>Manufacturer</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_USER_DATA_01</ID>
              <Code>177</Code>
              <IDAndCode>COMPENSATION_CONFIG [0xB1]</IDAndCode>
              <ValueText>SEL_GMV: 1; SEL_GMI: 2; SEL_RVV: 16; SEL_INTV: 1; SEL_CPV: 1; SEL_RVI: 8; SEL_INTI: 9; SEL_CPI: 3; SEL_RINTI: 0;</ValueText>
              <ValueEncoded xsi:type="PMBusBlock" Hex="0x1240422246" />
              <ParameterType>Raw</ParameterType>
              <ParameterCategory>User</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>FREQUENCY_SWITCH</ID>
              <Code>51</Code>
              <IDAndCode>FREQUENCY_SWITCH [0x33]</IDAndCode>
              <ValueText>550 kHz</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0226" />
              <ValueNumeric>550</ValueNumeric>
              <ParameterType>Frequency</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IC_DEVICE_ID</ID>
              <Code>173</Code>
              <IDAndCode>IC_DEVICE_ID [0xAD]</IDAndCode>
              <ValueText>0x5449546D2441 (TPS546D24A)</ValueText>
              <ValueEncoded xsi:type="PMBusBlock" Hex="0x5449546D2441" />
              <ParameterType>Raw</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IC_DEVICE_REV</ID>
              <Code>174</Code>
              <IDAndCode>IC_DEVICE_REV [0xAE]</IDAndCode>
              <ValueText>0x4000</ValueText>
              <ValueEncoded xsi:type="PMBusBlock" Hex="0x4000" />
              <ParameterType>Raw</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_INTERLEAVE</ID>
              <Code>55</Code>
              <IDAndCode>INTERLEAVE [0x37]</IDAndCode>
              <ValueText>Group ID: 0; Num Group: 2; Interleave Order: 0 (0°)</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0020" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_CAL_GAIN</ID>
              <Code>56</Code>
              <IDAndCode>IOUT_CAL_GAIN  phase ALL [0x38]</IDAndCode>
              <ValueText>1.000 </ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xC880" />
              <ValueNumeric>1</ValueNumeric>
              <ParameterType>Ratio</ParameterType>
              <ParameterCategory>Calibration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_CAL_OFFSET</ID>
              <Code>57</Code>
              <IDAndCode>IOUT_CAL_OFFSET  phase ALL [0x39]</IDAndCode>
              <ValueText>0.0000 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xE000" />
              <ValueNumeric>0</ValueNumeric>
              <ParameterType>CurrentCalibration</ParameterType>
              <ParameterCategory>Calibration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_OC_FAULT_LIMIT</ID>
              <Code>70</Code>
              <IDAndCode>IOUT_OC_FAULT_LIMIT  phase ALL [0x46]</IDAndCode>
              <ValueText>104.00 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF8D0" />
              <ValueNumeric>104</ValueNumeric>
              <ParameterType>Current</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_OC_FAULT_RESPONSE</ID>
              <Code>71</Code>
              <IDAndCode>IOUT_OC_FAULT_RESPONSE  phase ALL [0x47]</IDAndCode>
              <ValueText>Response=3,Restart=7,Delay=7</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0xFF" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_OC_WARN_LIMIT</ID>
              <Code>74</Code>
              <IDAndCode>IOUT_OC_WARN_LIMIT  phase ALL [0x4A]</IDAndCode>
              <ValueText>80.00 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF8A0" />
              <ValueNumeric>80</ValueNumeric>
              <ParameterType>Current</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>MFR_ID</ID>
              <Code>153</Code>
              <IDAndCode>MFR_ID [0x99]</IDAndCode>
              <ValueText>0x005449</ValueText>
              <ValueEncoded xsi:type="PMBusBlock" Hex="0x005449" />
              <ParameterType>String</ParameterType>
              <ParameterCategory>Manufacturer</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>MFR_MODEL</ID>
              <Code>154</Code>
              <IDAndCode>MFR_MODEL [0x9A]</IDAndCode>
              <ValueText>0x000000</ValueText>
              <ValueEncoded xsi:type="PMBusBlock" Hex="0x000000" />
              <ParameterType>String</ParameterType>
              <ParameterCategory>Manufacturer</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>MFR_REVISION</ID>
              <Code>155</Code>
              <IDAndCode>MFR_REVISION [0x9B]</IDAndCode>
              <ValueText>0x000000</ValueText>
              <ValueEncoded xsi:type="PMBusBlock" Hex="0x000000" />
              <ParameterType>String</ParameterType>
              <ParameterCategory>Manufacturer</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>MFR_SERIAL</ID>
              <Code>158</Code>
              <IDAndCode>MFR_SERIAL [0x9E]</IDAndCode>
              <ValueText>0x000000</ValueText>
              <ValueEncoded xsi:type="PMBusBlock" Hex="0x000000" />
              <ParameterType>String</ParameterType>
              <ParameterCategory>Manufacturer</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_MFR_SPECIFIC_29</ID>
              <Code>237</Code>
              <IDAndCode>MISC_OPTIONS [MFR 29,0xED]</IDAndCode>
              <ValueText>PEC: False; Reset Vout: 0; Reset#: False; Vout Source: 0; Fault Count: False; ADC Resolution: 12; PullUp#: False</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0000" />
              <ParameterType>UnitlessZeroDigit</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_MFR_SPECIFIC_32</ID>
              <Code>240</Code>
              <IDAndCode>NVM_CHECKSUM [MFR 32,0xF0]</IDAndCode>
              <ValueText>Checksum: 08AF</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x08AF" />
              <ParameterType>UnitlessZeroDigit</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>ON_OFF_CONFIG</ID>
              <Code>2</Code>
              <IDAndCode>ON_OFF_CONFIG  phase ALL [0x02]</IDAndCode>
              <ValueText>Mode: CONTROL Pin Only; Control: Active High, Turn off Immediately</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x17" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>OnOff</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>OPERATION</ID>
              <Code>1</Code>
              <IDAndCode>OPERATION [0x01]</IDAndCode>
              <ValueText>Unit: ImmediateOff; Margin: None (IgnoreFault)</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x04" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>OnOff</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>OT_FAULT_LIMIT</ID>
              <Code>79</Code>
              <IDAndCode>OT_FAULT_LIMIT  phase ALL [0x4F]</IDAndCode>
              <ValueText>150 °C</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0096" />
              <ValueNumeric>150</ValueNumeric>
              <ParameterType>Temperature</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>OT_FAULT_RESPONSE</ID>
              <Code>80</Code>
              <IDAndCode>OT_FAULT_RESPONSE  phase ALL [0x50]</IDAndCode>
              <ValueText>Response=2,Restart=7,Delay=4</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0xBC" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>OT_WARN_LIMIT</ID>
              <Code>81</Code>
              <IDAndCode>OT_WARN_LIMIT  phase ALL [0x51]</IDAndCode>
              <ValueText>125 °C</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x007D" />
              <ValueNumeric>125</ValueNumeric>
              <ParameterType>Temperature</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_MFR_SPECIFIC_19</ID>
              <Code>227</Code>
              <IDAndCode>PGOOD_CONFIG [MFR 19,0xE3]</IDAndCode>
              <ValueText>PGood On Delay: 0, PGood Off Delay: 0; OVF Mask: True; OVW Mask: False; UVW Mask: False; UVF Mask: True; OCW Mask: True; OCF Mask: True; VIN_OVW Mask: True; VIN_OVF Mask: True</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x009F" />
              <ParameterType>UnitlessZeroDigit</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_MFR_SPECIFIC_30</ID>
              <Code>238</Code>
              <IDAndCode>PIN_DETECT_OVERRIDE [MFR 30,0xEE]</IDAndCode>
              <ValueText>Stack Config: True; Sync Config: True; Transient Reduction: True; Compensation: True; PMBus Address: True; Interleave: True;Fault Response: False; Ton Rise: True; Iout OC Fault Limit/Warn: True; Frequency Switch: True; Vout Command/Scale Loop: True</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x1F2F" />
              <ParameterType>UnitlessZeroDigit</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>PMBUS_REVISION</ID>
              <Code>152</Code>
              <IDAndCode>PMBUS_REVISION [0x98]</IDAndCode>
              <ValueText>1.3,1.3 - Part I: 1.3, Part II: 1.3</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x33" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>Manufacturer</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_USER_DATA_05</ID>
              <Code>181</Code>
              <IDAndCode>POWER_STAGE_CONFIG [0xB5]</IDAndCode>
              <ValueText>Gate Voltage: 4.7V;</ValueText>
              <ValueEncoded xsi:type="PMBusBlock" Hex="0x70" />
              <ParameterType>Raw</ParameterType>
              <ParameterCategory>User</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_IOUT</ID>
              <Code>140</Code>
              <IDAndCode>READ_IOUT  phase ALL [0x8C]</IDAndCode>
              <ValueText>-2.14 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xC5DD" />
              <ValueNumeric>-2.14</ValueNumeric>
              <ParameterType>Current</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_TEMPERATURE_1</ID>
              <Code>141</Code>
              <IDAndCode>READ_TEMPERATURE_1  phase ALL [0x8D]</IDAndCode>
              <ValueText>32 °C</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0020" />
              <ValueNumeric>32</ValueNumeric>
              <ParameterType>Temperature</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_VIN</ID>
              <Code>136</Code>
              <IDAndCode>READ_VIN  phase ALL [0x88]</IDAndCode>
              <ValueText>12.078 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xD305" />
              <ValueNumeric>12.078</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_VOUT</ID>
              <Code>139</Code>
              <IDAndCode>READ_VOUT  phase ALL [0x8B]</IDAndCode>
              <ValueText>0.794922 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0197" />
              <ValueNumeric>0.794921875</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_MFR_SPECIFIC_33</ID>
              <Code>241</Code>
              <IDAndCode>SIMULATE_FAULT [MFR 33,0xF1]</IDAndCode>
              <ValueText>Persist Fault: False; Temp OTF: False; Iout OCF: False; Vin Off: False; Vin OVF: False; Vout UVF: False; Vout OVF: False; Persist Warn: False; Iout OCW: False; Vin UVW: False; Vin OVW: False; Vout UVW: False; Vout OVW: False</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0000" />
              <ParameterType>UnitlessZeroDigit</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_MFR_SPECIFIC_31</ID>
              <Code>239</Code>
              <IDAndCode>SLAVE_ADDRESS [MFR 31,0xEF]</IDAndCode>
              <ValueText>Address: 0x14 (20d)</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x14" />
              <ParameterType>UnitlessZeroDigit</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>SMBALERT_MASK_CML</ID>
              <Code>27</Code>
              <IDAndCode>SMBALERT_MASK_CML [0x1B]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>SMBALERT_MASK_INPUT</ID>
              <Code>27</Code>
              <IDAndCode>SMBALERT_MASK_INPUT [0x1B]</IDAndCode>
              <ValueText>UNIT_OFF_FOR_INSUFFICIENT_VIN,VIN_UV_WARN,VIN_OV_WARN,VIN_OV_FAULT</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0xE8" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>SMBALERT_MASK_IOUT</ID>
              <Code>27</Code>
              <IDAndCode>SMBALERT_MASK_IOUT [0x1B]</IDAndCode>
              <ValueText>CURRENT_SHARE_FAULT,IOUT_UC_FAULT</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x18" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>SMBALERT_MASK_MFR_SPECIFIC</ID>
              <Code>27</Code>
              <IDAndCode>SMBALERT_MASK_MFR_SPECIFIC [0x1B]</IDAndCode>
              <ValueText>MFR1,MFR6</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x42" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>SMBALERT_MASK_OTHER</ID>
              <Code>27</Code>
              <IDAndCode>SMBALERT_MASK_OTHER [0x1B]</IDAndCode>
              <ValueText>RESERVED0</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x01" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>SMBALERT_MASK_TEMPERATURE</ID>
              <Code>27</Code>
              <IDAndCode>SMBALERT_MASK_TEMPERATURE [0x1B]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>SMBALERT_MASK_VOUT</ID>
              <Code>27</Code>
              <IDAndCode>SMBALERT_MASK_VOUT [0x1B]</IDAndCode>
              <ValueText>TOFF_MAX_WARN</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x02" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_MFR_SPECIFIC_28</ID>
              <Code>236</Code>
              <IDAndCode>STACK_CONFIG [MFR 28,0xEC]</IDAndCode>
              <ValueText>Bcx Stop: 1; Bcx Start: 0</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0001" />
              <ParameterType>UnitlessZeroDigit</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_BYTE</ID>
              <Code>120</Code>
              <IDAndCode>STATUS_BYTE [0x78]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_CML</ID>
              <Code>126</Code>
              <IDAndCode>STATUS_CML [0x7E]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_INPUT</ID>
              <Code>124</Code>
              <IDAndCode>STATUS_INPUT [0x7C]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_IOUT</ID>
              <Code>123</Code>
              <IDAndCode>STATUS_IOUT [0x7B]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_MFR_SPECIFIC</ID>
              <Code>128</Code>
              <IDAndCode>STATUS_MFR_SPECIFIC [0x80]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_OTHER</ID>
              <Code>127</Code>
              <IDAndCode>STATUS_OTHER [0x7F]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_TEMPERATURE</ID>
              <Code>125</Code>
              <IDAndCode>STATUS_TEMPERATURE [0x7D]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_VOUT</ID>
              <Code>122</Code>
              <IDAndCode>STATUS_VOUT [0x7A]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_WORD</ID>
              <Code>121</Code>
              <IDAndCode>STATUS_WORD [0x79]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0000" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_MFR_SPECIFIC_20</ID>
              <Code>228</Code>
              <IDAndCode>SYNC_CONFIG [MFR 20,0xE4]</IDAndCode>
              <ValueText>SYNC_DIR: Auto Detect SYNC (0x03); SYNC_EDGE: Synchronize to rising edge of SYNC (True))</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0xF0" />
              <ParameterType>UnitlessZeroDigit</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TPSCATFISH_MFR_SPECIFIC_00</ID>
              <Code>208</Code>
              <IDAndCode>TELEMETRY_CONFIG [MFR 00,0xD0]</IDAndCode>
              <ValueText>VOUT: Priority: 0x00; Avg_Num: 0x03;IOUT: Priority: 0x00; Avg_Num: 0x03;TEMPERATURE: Priority: 0x00; Avg_Num: 0x03;VIN: Priority: 0x00; Avg_Num: 0x03</ValueText>
              <ValueEncoded xsi:type="PMBusBlock" Hex="0x030303030003" />
              <ParameterType>Raw</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TOFF_DELAY</ID>
              <Code>100</Code>
              <IDAndCode>TOFF_DELAY [0x64]</IDAndCode>
              <ValueText>0.0 ms</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF800" />
              <ValueNumeric>0</ValueNumeric>
              <ParameterType>TimeOneDigitMilliseconds</ParameterType>
              <ParameterCategory>OnOff</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TOFF_FALL</ID>
              <Code>101</Code>
              <IDAndCode>TOFF_FALL [0x65]</IDAndCode>
              <ValueText>0.50 ms</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF002" />
              <ValueNumeric>0.5</ValueNumeric>
              <ParameterType>TimeOneDigitMilliseconds</ParameterType>
              <ParameterCategory>OnOff</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TON_DELAY</ID>
              <Code>96</Code>
              <IDAndCode>TON_DELAY [0x60]</IDAndCode>
              <ValueText>0.0 ms</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF800" />
              <ValueNumeric>0</ValueNumeric>
              <ParameterType>TimeOneDigitMilliseconds</ParameterType>
              <ParameterCategory>OnOff</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TON_MAX_FAULT_LIMIT</ID>
              <Code>98</Code>
              <IDAndCode>TON_MAX_FAULT_LIMIT [0x62]</IDAndCode>
              <ValueText>&lt;No Limit&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF800" />
              <ValueNumeric>0</ValueNumeric>
              <ParameterType>TimeOneDigitMilliseconds</ParameterType>
              <ParameterCategory>OnOff</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TON_MAX_FAULT_RESPONSE</ID>
              <Code>99</Code>
              <IDAndCode>TON_MAX_FAULT_RESPONSE [0x63]</IDAndCode>
              <ValueText>Response=0,Restart=7,Delay=3</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x3B" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>OnOff</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>TON_RISE</ID>
              <Code>97</Code>
              <IDAndCode>TON_RISE [0x61]</IDAndCode>
              <ValueText>3.00 ms</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF00C" />
              <ValueNumeric>3</ValueNumeric>
              <ParameterType>TimeOneDigitMilliseconds</ParameterType>
              <ParameterCategory>OnOff</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VIN_OFF</ID>
              <Code>54</Code>
              <IDAndCode>VIN_OFF  phase ALL [0x36]</IDAndCode>
              <ValueText>2.50 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF00A" />
              <ValueNumeric>2.5</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VIN_ON</ID>
              <Code>53</Code>
              <IDAndCode>VIN_ON  phase ALL [0x35]</IDAndCode>
              <ValueText>2.75 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF00B" />
              <ValueNumeric>2.75</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VIN_OV_FAULT_LIMIT</ID>
              <Code>85</Code>
              <IDAndCode>VIN_OV_FAULT_LIMIT [0x55]</IDAndCode>
              <ValueText>21 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0015" />
              <ValueNumeric>21</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VIN_OV_FAULT_RESPONSE</ID>
              <Code>86</Code>
              <IDAndCode>VIN_OV_FAULT_RESPONSE [0x56]</IDAndCode>
              <ValueText>Response=0,Restart=7,Delay=4</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x3C" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VIN_UV_WARN_LIMIT</ID>
              <Code>88</Code>
              <IDAndCode>VIN_UV_WARN_LIMIT [0x58]</IDAndCode>
              <ValueText>2.50 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF00A" />
              <ValueNumeric>2.5</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_COMMAND</ID>
              <Code>33</Code>
              <IDAndCode>VOUT_COMMAND [0x21]</IDAndCode>
              <ValueText>0.798828 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0199" />
              <ValueNumeric>0.798828125</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_MARGIN_HIGH</ID>
              <Code>37</Code>
              <IDAndCode>VOUT_MARGIN_HIGH [0x25]</IDAndCode>
              <ValueText>0.839394 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x021A" />
              <ValueNumeric>0.839393615722656</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_MARGIN_LOW</ID>
              <Code>38</Code>
              <IDAndCode>VOUT_MARGIN_LOW [0x26]</IDAndCode>
              <ValueText>0.758263 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x01E6" />
              <ValueNumeric>0.758262634277344</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_MAX</ID>
              <Code>36</Code>
              <IDAndCode>VOUT_MAX [0x24]</IDAndCode>
              <ValueText>1.500000 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0300" />
              <ValueNumeric>1.5</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_MIN</ID>
              <Code>43</Code>
              <IDAndCode>VOUT_MIN [0x2B]</IDAndCode>
              <ValueText>0.500000 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0100" />
              <ValueNumeric>0.5</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_OV_FAULT_LIMIT</ID>
              <Code>64</Code>
              <IDAndCode>VOUT_OV_FAULT_LIMIT [0x40]</IDAndCode>
              <ValueText>0.917404 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x024C" />
              <ValueNumeric>0.917404174804688</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_OV_FAULT_RESPONSE</ID>
              <Code>65</Code>
              <IDAndCode>VOUT_OV_FAULT_RESPONSE [0x41]</IDAndCode>
              <ValueText>Response=2,Restart=7,Delay=5</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0xBD" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_OV_WARN_LIMIT</ID>
              <Code>66</Code>
              <IDAndCode>VOUT_OV_WARN_LIMIT [0x42]</IDAndCode>
              <ValueText>0.870598 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x022E" />
              <ValueNumeric>0.870597839355469</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_SCALE_LOOP</ID>
              <Code>41</Code>
              <IDAndCode>VOUT_SCALE_LOOP [0x29]</IDAndCode>
              <ValueText>0.500 </ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xC840" />
              <ValueNumeric>0.5</ValueNumeric>
              <ParameterType>UnitlessThreeDigit</ParameterType>
              <ParameterCategory>Calibration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_TRANSITION_RATE</ID>
              <Code>39</Code>
              <IDAndCode>VOUT_TRANSITION_RATE [0x27]</IDAndCode>
              <ValueText>1.0000 mV/μs</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xE010" />
              <ValueNumeric>1</ValueNumeric>
              <ParameterType>Transition</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_TRIM</ID>
              <Code>34</Code>
              <IDAndCode>VOUT_TRIM [0x22]</IDAndCode>
              <ValueText>0.000000 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0000" />
              <ValueNumeric>0</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Calibration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_UV_FAULT_LIMIT</ID>
              <Code>68</Code>
              <IDAndCode>VOUT_UV_FAULT_LIMIT [0x44]</IDAndCode>
              <ValueText>0.678692 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x01B3" />
              <ValueNumeric>0.678691864013672</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_UV_FAULT_RESPONSE</ID>
              <Code>69</Code>
              <IDAndCode>VOUT_UV_FAULT_RESPONSE [0x45]</IDAndCode>
              <ValueText>Response=2,Restart=7,Delay=6</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0xBE" />
              <ParameterType>Custom</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>VOUT_UV_WARN_LIMIT</ID>
              <Code>67</Code>
              <IDAndCode>VOUT_UV_WARN_LIMIT [0x43]</IDAndCode>
              <ValueText>0.727058 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x01D2" />
              <ValueNumeric>0.727058410644531</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>WRITE_PROTECT</ID>
              <Code>16</Code>
              <IDAndCode>WRITE_PROTECT [0x10]</IDAndCode>
              <ValueText>0</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Raw</ParameterType>
              <ParameterCategory>Configuration</ParameterCategory>
              <Page>255</Page>
              <Phase xsi:nil="true" />
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_CAL_GAIN_1</ID>
              <Code>56</Code>
              <IDAndCode>IOUT_CAL_GAIN_1 [0x38]</IDAndCode>
              <ValueText>1.000 </ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xC880" />
              <ValueNumeric>1</ValueNumeric>
              <ParameterType>Ratio</ParameterType>
              <ParameterCategory>Calibration</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_CAL_OFFSET_1</ID>
              <Code>57</Code>
              <IDAndCode>IOUT_CAL_OFFSET phase 1 (0x00) [0x39]</IDAndCode>
              <ValueText>0.0000 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xE000" />
              <ValueNumeric>0</ValueNumeric>
              <ParameterType>CurrentCalibration</ParameterType>
              <ParameterCategory>Calibration</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_OC_FAULT_LIMIT_1</ID>
              <Code>70</Code>
              <IDAndCode>IOUT_OC_FAULT_LIMIT phase 1 (0x00) [0x46]</IDAndCode>
              <ValueText>52.00 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF0D0" />
              <ValueNumeric>52</ValueNumeric>
              <ParameterType>Current</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_OC_WARN_LIMIT_1</ID>
              <Code>74</Code>
              <IDAndCode>IOUT_OC_WARN_LIMIT phase 1 (0x00) [0x4A]</IDAndCode>
              <ValueText>40.00 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF0A0" />
              <ValueNumeric>40</ValueNumeric>
              <ParameterType>Current</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>OT_FAULT_LIMIT_1</ID>
              <Code>79</Code>
              <IDAndCode>OT_FAULT_LIMIT phase 1 (0x00) [0x4F]</IDAndCode>
              <ValueText>150 °C</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0096" />
              <ValueNumeric>150</ValueNumeric>
              <ParameterType>Temperature</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>OT_WARN_LIMIT_1</ID>
              <Code>81</Code>
              <IDAndCode>OT_WARN_LIMIT phase 1 (0x00) [0x51]</IDAndCode>
              <ValueText>125 °C</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x007D" />
              <ValueNumeric>125</ValueNumeric>
              <ParameterType>Temperature</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_IOUT_1</ID>
              <Code>140</Code>
              <IDAndCode>READ_IOUT phase 1 (0x00) [0x8C]</IDAndCode>
              <ValueText>-1.04 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xBDEE" />
              <ValueNumeric>-1.04</ValueNumeric>
              <ParameterType>Current</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_TEMPERATURE_1_1</ID>
              <Code>141</Code>
              <IDAndCode>READ_TEMPERATURE_1 phase 1 (0x00) [0x8D]</IDAndCode>
              <ValueText>32 °C</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xDBF0" />
              <ValueNumeric>32</ValueNumeric>
              <ParameterType>Temperature</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_VIN_1</ID>
              <Code>136</Code>
              <IDAndCode>READ_VIN phase 1 (0x00) [0x88]</IDAndCode>
              <ValueText>12.094 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xD306" />
              <ValueNumeric>12.094</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_VOUT_1</ID>
              <Code>139</Code>
              <IDAndCode>READ_VOUT phase 1 (0x00) [0x8B]</IDAndCode>
              <ValueText>0.794922 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0197" />
              <ValueNumeric>0.794921875</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_CML_1</ID>
              <Code>126</Code>
              <IDAndCode>STATUS_CML_1 [0x7E]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_INPUT_1</ID>
              <Code>124</Code>
              <IDAndCode>STATUS_INPUT_1 [0x7C]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_IOUT_1</ID>
              <Code>123</Code>
              <IDAndCode>STATUS_IOUT_1 [0x7B]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_MFR_SPECIFIC_1</ID>
              <Code>128</Code>
              <IDAndCode>STATUS_MFR_SPECIFIC_1 [0x80]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_TEMPERATURE_1</ID>
              <Code>125</Code>
              <IDAndCode>STATUS_TEMPERATURE_1 [0x7D]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>0</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_CAL_GAIN_2</ID>
              <Code>56</Code>
              <IDAndCode>IOUT_CAL_GAIN_2 [0x38]</IDAndCode>
              <ValueText>1.000 </ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xC880" />
              <ValueNumeric>1</ValueNumeric>
              <ParameterType>Ratio</ParameterType>
              <ParameterCategory>Calibration</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_CAL_OFFSET_2</ID>
              <Code>57</Code>
              <IDAndCode>IOUT_CAL_OFFSET phase 2 (0x01) [0x39]</IDAndCode>
              <ValueText>0.0000 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xE000" />
              <ValueNumeric>0</ValueNumeric>
              <ParameterType>CurrentCalibration</ParameterType>
              <ParameterCategory>Calibration</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_OC_FAULT_LIMIT_2</ID>
              <Code>70</Code>
              <IDAndCode>IOUT_OC_FAULT_LIMIT phase 2 (0x01) [0x46]</IDAndCode>
              <ValueText>52.00 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF0D0" />
              <ValueNumeric>52</ValueNumeric>
              <ParameterType>Current</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>IOUT_OC_WARN_LIMIT_2</ID>
              <Code>74</Code>
              <IDAndCode>IOUT_OC_WARN_LIMIT phase 2 (0x01) [0x4A]</IDAndCode>
              <ValueText>40.00 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xF0A0" />
              <ValueNumeric>40</ValueNumeric>
              <ParameterType>Current</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>OT_FAULT_LIMIT_2</ID>
              <Code>79</Code>
              <IDAndCode>OT_FAULT_LIMIT phase 2 (0x01) [0x4F]</IDAndCode>
              <ValueText>150 °C</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x0096" />
              <ValueNumeric>150</ValueNumeric>
              <ParameterType>Temperature</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>OT_WARN_LIMIT_2</ID>
              <Code>81</Code>
              <IDAndCode>OT_WARN_LIMIT phase 2 (0x01) [0x51]</IDAndCode>
              <ValueText>125 °C</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x007D" />
              <ValueNumeric>125</ValueNumeric>
              <ParameterType>Temperature</ParameterType>
              <ParameterCategory>Limits</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_IOUT_2</ID>
              <Code>140</Code>
              <IDAndCode>READ_IOUT phase 2 (0x01) [0x8C]</IDAndCode>
              <ValueText>-1.07 A</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xBDDE" />
              <ValueNumeric>-1.07</ValueNumeric>
              <ParameterType>Current</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_TEMPERATURE_1_2</ID>
              <Code>141</Code>
              <IDAndCode>READ_TEMPERATURE_1 phase 2 (0x01) [0x8D]</IDAndCode>
              <ValueText>31 °C</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xDBD8" />
              <ValueNumeric>31</ValueNumeric>
              <ParameterType>Temperature</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_VIN_2</ID>
              <Code>136</Code>
              <IDAndCode>READ_VIN phase 2 (0x01) [0x88]</IDAndCode>
              <ValueText>12.094 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0xD306" />
              <ValueNumeric>12.094</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>READ_VOUT_2</ID>
              <Code>139</Code>
              <IDAndCode>READ_VOUT phase 2 (0x01) [0x8B]</IDAndCode>
              <ValueText>0.923828 V</ValueText>
              <ValueEncoded xsi:type="PMBusWord" Hex="0x01D9" />
              <ValueNumeric>0.923828125</ValueNumeric>
              <ParameterType>Voltage</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_CML_2</ID>
              <Code>126</Code>
              <IDAndCode>STATUS_CML_2 [0x7E]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_INPUT_2</ID>
              <Code>124</Code>
              <IDAndCode>STATUS_INPUT_2 [0x7C]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_IOUT_2</ID>
              <Code>123</Code>
              <IDAndCode>STATUS_IOUT_2 [0x7B]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_MFR_SPECIFIC_2</ID>
              <Code>128</Code>
              <IDAndCode>STATUS_MFR_SPECIFIC_2 [0x80]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
            <Parameter>
              <ID>STATUS_TEMPERATURE_2</ID>
              <Code>125</Code>
              <IDAndCode>STATUS_TEMPERATURE_2 [0x7D]</IDAndCode>
              <ValueText>&lt;EMPTY&gt;</ValueText>
              <ValueEncoded xsi:type="PMBusByte" Hex="0x00" />
              <ParameterType>Bitmask</ParameterType>
              <ParameterCategory>Status</ParameterCategory>
              <Page>255</Page>
              <Phase>1</Phase>
              <CustomIndex xsi:nil="true" />
            </Parameter>
          </Parameters>
          <Hex_Data />
          <Custom xsi:type="CatfishProjectData">
            <Save_In_Offline_Mode>false</Save_In_Offline_Mode>
            <Write_To_NVM_Pending>true</Write_To_NVM_Pending>
            <Pin_Strapping_Info>
              <MSEL1>
                <R_Divider_Code>0</R_Divider_Code>
                <Rbot_Code>0</Rbot_Code>
                <Resistor>
                  <Resistor_Top>0</Resistor_Top>
                  <Resistor_Bot>0</Resistor_Bot>
                </Resistor>
                <FSW>275</FSW>
                <Compensation_Config>
                  <ILOOP_GAIN>-1</ILOOP_GAIN>
                  <VLOOP_GAIN>-1</VLOOP_GAIN>
                  <Rbot_Code>255</Rbot_Code>
                  <FSW>-1</FSW>
                  <RDiv_Code>255</RDiv_Code>
                </Compensation_Config>
              </MSEL1>
              <MSEL2>
                <R_Divider_Code>0</R_Divider_Code>
                <Rbot_Code>0</Rbot_Code>
                <Resistor>
                  <Resistor_Top>21500</Resistor_Top>
                  <Resistor_Bot>4640</Resistor_Bot>
                </Resistor>
                <Number_Of_Slaves>0</Number_Of_Slaves>
                <TON_RISE>0</TON_RISE>
                <OC_Fault_And_Warn>
                  <IOUT_OC_FAULT_LIMIT>52</IOUT_OC_FAULT_LIMIT>
                  <IOUT_OC_WARN_LIMIT>40</IOUT_OC_WARN_LIMIT>
                  <TON_RISE xsi:nil="true" />
                  <Number_Of_Slaves xsi:nil="true" />
                  <Max_OC_FAULT_LIMIT>52</Max_OC_FAULT_LIMIT>
                  <Min_OC_FAULT_LIMIT>52</Min_OC_FAULT_LIMIT>
                </OC_Fault_And_Warn>
              </MSEL2>
              <VSEL>
                <R_Divider_Code>0</R_Divider_Code>
                <Rbot_Code>0</Rbot_Code>
                <Resistor>
                  <Resistor_Top>0</Resistor_Top>
                  <Resistor_Bot>0</Resistor_Bot>
                </Resistor>
                <VOUT_COMMAND>-1</VOUT_COMMAND>
                <VOUT_MAX>-1</VOUT_MAX>
                <VOUT_MIN>-1</VOUT_MIN>
                <VOUT_SCALE_LOOP>0</VOUT_SCALE_LOOP>
              </VSEL>
              <ADDRSEL>
                <R_Divider_Code>0</R_Divider_Code>
                <Rbot_Code>0</Rbot_Code>
                <Resistor>
                  <Resistor_Top>0</Resistor_Top>
                  <Resistor_Bot>0</Resistor_Bot>
                </Resistor>
                <Slave_Address>0</Slave_Address>
                <Sync>Auto</Sync>
                <PHASE_SHIFT>0</PHASE_SHIFT>
                <INTERLEAVE>0</INTERLEAVE>
              </ADDRSEL>
              <Pin_Strapping />
            </Pin_Strapping_Info>
          </Custom>
        </Device>
      </Devices>
      <Use_Old_UCD92XX_CLA_Gains>true</Use_Old_UCD92XX_CLA_Gains>
    </ProjectData>

    2. Open the Fusion Digital Power Designer and select 'Offline Mode'

    3. Select 'Create new Offline system by opening existing system file'

    4. Click 'Select File' and navigate to the location where you have saved the system file

    5. Select 'Finish'. When the next window opens up, select 'Click to configure' to open the device GUI

    I have an evaluation board for the TPSM8D6B24 being shipped to me right now; due to the upcoming holiday, I may not be able to evaluate the hardware until the middle of next week. I will make sure that the B24 module is supported and I will update you here next week.

    Best regards,

    Britton

  • Hello Torben,

    I confirmed that TPSM8D6B24 is supported. When detecting a TPSM8D6B24 device, Fusion will display the part ID for TPSM8D6C24 as they have the same user interface. This user interface is also the same for TPS546D24A, so if you are using offline mode you can select the TPS546D24A from the list of available parts. I will close this ticket now

    Best regards,

    Britton