This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: BQ25606RGER pin state in Charging disable mode.

Part Number: BQ25606

Hi,

Could you please advise what the recommended state of the below pins, when the charger is permanently disabled (CE=HIGH), OTG is not used and BQ25606RGER is used in the Supplement Mode with EXT VBUS 5-9V and BAT input voltage 4.4V?

OTG - GND/Open?

VSET- Open/GND/PD? should it be set up to the actual BAT voltage?

ICHG - GND/Open/PD? 

Regards

Vitaliy