Other Parts Discussed in Thread: BQ76942
Hi TI team,
The BQ25756 charge controller we intend to use with a battery pack: LiFePo4 8S1P 29.2V battery.
Can you describe any way to use this charge controller by just triggering input pins?
I have read the manual and it appears that charge cycles can only start when amongst other things, the EN_CHG bit on REG0x17 is set to 1 via I2C.
For our setup we had intended to use the BQ25756 with a BQ76942. In this related post I've extrapolated that these two ICs will be compatible.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1281031/bq25756-can-we-use-bq25756-vith-bq7694?tisearch=e2e-sitesearch&keymatch=BQ25756#
If there is a way to operate the BQ25756 without I2C, can you confirm that the BQ76942 will work well in combination with the BQ25756 IC?
If there is no way to operate the BQ25756 without I2C can you suggest any other LiFePo4 charge controllers which don't require I2C to operate, which are compatible with the BQ76942?
Thank you,
Regards
Hiroshi Ransom