Part Number: LM5143
Other Parts Discussed in Thread: LM5148
Hi,
If we use LM5143 in single output two phase application. Does it also support PFM or ultra low Iq mode?
I only seem datasheet shows it in dual output operation.

Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeff,
The LM(2)5143/-Q1 does not have ultra-low quiescent current in 2-phase configuration (with MODE tied high). It will enter pulse skipping at light load but not achieve the super low quiescent current normally achieved with the dual-output setting. If this is needed, please consider two LM5148 controllers as a 2-phase configuration -- this has the added benefit of 80V input capability.
Regards,
Tim
Hi Tim,
One more quesiton, In datasheet table10-7, 2 phase application.
Use Onsemi MOSFET. I have found TI MOSFET alternative parts below.
Does it have any impact or need take care?
NVMFS5C673NL
NVMFS5C628NL

Thanks!
Jeff