Part Number: TPS7H1111-SEP
Other Parts Discussed in Thread: TPS7H1111EVM-CVAL,
Hello. The TPS7H1111EVM-CVAL board has a 51 ohm resistor between the voltage output and OUTS pin for Bode plot measurements. The TPS7H1111 datasheet (Section 8.3.8) states that any such resistor should be replaced with a 0 ohm shunt during nominal operation. Can you confirm that this is required, rather than leaving the resistor in place during nominal operation? If this is the case, how will the results I see with the evaluation board be affected by the 51 ohm resistor and should I replace this with 0 ohms for my other measurements?
When using two parallel TPS7H1111-SEP devices with current sharing, are there any other considerations to be taken into account when taking Bode plot measurements, or is it sufficient to take the measurements for each device separately using a resistor between OUT and OUTS for each device?
Thanks,
David