This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: Recommend suitable IC

Part Number: TL431

Hi BU expert,

Does TI have voltage reference chip which the referent voltage is 2.2V? Thanks.

Regards,

Charlie

  • Hello Charlie,

    We do not have a device with a fixed output of 2.2V but you can use an adjustable device such as TLVH431 to set the output to 2.2V.

    You can use this circuit and select R1 and R2 to get 2.2V

    Thanks,

    Walter