This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck converter design



Hi Team,

My Design inputs:-

  1. input voltage range 1:- Vin min:316 Vdc, Vin nominal:587Vdc, Vin Max: 815Vdc
  2. input voltage range 2:- Vin min:417 Vdc, Vin nominal:700Vdc, Vin Max: 1000Vdc
  3. input voltage range 3:- Vin min:417Vdc, Vin nominal:800Vdc, Vin Max: 1200Vdc

output remains common for 3 diffrent input voltage range

  1. Vout::300Vdc
  2. Iout:2.26Adc
  3. Pout:626W

I want to use conventional Buck converter(Not synchronous buck) so please help me for best pwm ic and suggest me best Design application note.