This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
Thank you for reaching out,
I have the concern regarding your output capacitor value. I see a 3* 22uF & 1* 10uF in the schematic, As per the datasheet recommendations the maximum Cout value is 2*22uF considering the effective capacitance can vary by +20% and -50%. In case the customer want to use the Cout value out of the datasheet recommendations, then they need to evaluate the stability of the device.
If we change the output capacitor size from 0805 to 0603, is there have any side effect?
There should be any problem as far as the Cout value is within the above recommendation.
Thank you & regards,
Moheddin.
Hello Jimmy,
If you don't have any further questions can you please close the thread by clicking on Resolved.
Thank you & regards,
Moheddin.