Hi Sir,
We have problems in the application of LM5176. Due to our EMI requirements, we need to add an inductor PL4 (200uH/4A) at the input, as shown in the red circle in Figure 1 attached. In our application, LM5176 Vin=5V~36V, VOUT=8.25V (Tool is in the attachment). this problem is that when load on the output, the Vin voltage will have unstable resonance, as shown in Figures 3 and 4 attached. Different loads will also appear at different voltage.
The voltage is unstable (as shown in Figure 5). This problem was only seen after adding an inductor(PL4). Only when the inductor is paired with the LM5176 circuit can it be seen (the same for EVM test.).
we would like to ask your comment. Does your experience suggest any solutions? The schematic and test waveform is in the attachment. The current test as below:
1. we try add E-Cap to Vin, and it improved. However, the space height is limited and it is impossible to add this type of E-capacitor.
2. To use MLCC Cap, we need to add at least 32pcs 10u/50V, but the space is limited and it is impossible to add so many capacitors.
3. Reduce the filter inductance(PL4) value to 150 uH no much improvement (<150uH does not help much with EMI).
LM5176 test report.xlsxAC FLEET.PDFLM5176 Buck-Boost Quickstart Tool_Joe_1208.xlsm