This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24170: BQ24170

Part Number: BQ24170


Hi

The TS pin is OF  BQ24170 is connected to resistors including a NTC 10kohm RESISTOR  / THERMISTOR in order to prevent high temperature of the battery.

Is it right to attach it to the battery? If it is attached to the BQ24170 it controls is temperature of the component and not the battery.

Thanks