Hi expert,
I found that the secondary side turn ratio of Load 2/3 doesn't change as input voltage and max duty circle varies? Is that right?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
I found that the secondary side turn ratio of Load 2/3 doesn't change as input voltage and max duty circle varies? Is that right?
Hi Jass,
Thanks for using the e2e forum.
If I understand your observations correctly, this should not be an error.
The winding ratios and output voltage results of load 2 & 3 are depending on the regulated rail, which is load 1.
The flyback controller can only regulate one rail actively (load 1), the other two (or any additional winding) will be indirectly regulated via the winding ratio of the transformer.
We have a lot of resources on flyback design in general. One example would be this app note:
https://www.ti.com/seclit/ml/slup261/slup261.pdf
I hope this explanation is helpful.
Best regards,
Niklas
You can see in the table, the calculated ratio of load 1 is 0.89 while the other 2 is 0.5, but they output the same voltage, is it right?