Hi team,
Could you please advise the min/typ/max standoff of TPS7B7701/2 device below?
regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you please advise the min/typ/max standoff of TPS7B7701/2 device below?
regards,
Hi Shinji,
You can see the measurement of the standoff on the data sheet as you attached. Can you please elaborate on the additional information you would like?
Thank you,
Josh
Dear Josh,
In order to optimize the solder mask opening ratio of the THERMAL PAD,
I would like to know the actual value of 0.15/0.05.
Best Regards,
Hi Taichi,
I have reached out to the packaging team on this request and I'll let you know when I have a response. Please be aware that it may take 1-2 weeks.
Thanks,
Stephen
Dear Stephen
Thank you for your response.
However, this is very urgent and necessary information, so I would like to ask you to provide it early.
Thank you for your consideration.
Best Regards,
Thanks Taichi, as soon as I hear back from the packaging team I will let you know.
Thanks,
Stephen
Hi Taichi,
I heard back much quicker than expected from the packaging team. Here is their response:
"TI follows JEDEC spec for MO-153 package standoff of 0.05-0.15mm. TI suggests customers to fabricate the stencil with 0.125mm thickness. With 0.125mm thick stencil there should be no issue to have the component thermal pad solder onto the PCB."
Thanks,
Stephen
Dear Stephen
Thank you for your response.
I understand that it is JEDEC compliant, but I would like to know the actual value.
Could you please provide us with the following information?
・Variation in standoffs
・Process Capability Index (Cpk)
Best Regards,
Hi Taichi,
We typically cannot provide Cpk values or things of that nature as that offers insight into our proprietary design processes. Even still, I'll reach out to packaging again to obtain their reply.
Thanks,
Stephen
Hi Taichi,
We can provide the following information:
Number of Samples : 458272
Range : 0.0818 – 0.1267 mm
Average : 0.108mm
CPK : 2.127
Thanks,
Stephen
Dear Stephen
Thank you for your answer.
I review your answers.
If there is anything, I will contact you again.
Best Regars,