Hello Sir,
In the LM5177 datasheet, at first page, it says, switching frequency is fixed for all three modes. And also max frequency is 600kHz. But in the 8.3.6 Section, the switching frequency can be changed to 2.2MHz, and also it says, "the switching frequency can be dynamically changed during operation by changing the current flowing through the resistor" . And Fig.8-9 and 8-10 shows the ways to change the switching frequency. In fact, I prefer to change the switching frequency to get maximum performance. I want to ask you , is it possible? Our application specifications are below;
Vin : 10-55V
Vout : 24V
I out max : 7A
regards