This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25762-Q1: Is this IC capable of being configured with resistors?

Part Number: TPS25762-Q1


Hello,

I'm designing a board with very limited space, and am trying to eliminate as many extra components as possible.

Is the TPS25762-Q1 able to be programmed with only resistors?

Or, does the TPS25762-Q1 have a default configuration pre-loaded to it, that can be used instead of having to use an EEPROM or I2C?

The data sheet mostly refers to using the application GUI, but doesn't mention much about functionality without using the GUI.

My design is supposed to be used as a stand-alone PD charger for smart phones and cameras.

Thank you,