This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92602EVM: Operation questions

Part Number: TPS92602EVM


Hi team,

My customer do validating with EVM.

They set Rsns=300mOhm + Analog Dimming function so that Isns is limited 300mA.

When they input PWMIN=10%, EVM shows Open LED Detected but LED still light. Is this correct operation?

If correct, this is error description, right? V(isp-isn)=300mOhm*300mA*10%=9mV(Open LED Detected)

The data sheet says that Vdaig outputs the voltage according to the voltage V(isp-isn).
So, the output voltage of VDAIG is also output in a PWM-like waveform?

Regards,

Youhei MIYAOKA