Part Number: TPS7A02
Hi,
I am using TPS7A0230PDBVR, the datasheet note with capacitor output "22 µF is the maximum derated capacitance that can be used for stability".
What happen when i use 100uF.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS7A02
Hi,
I am using TPS7A0230PDBVR, the datasheet note with capacitor output "22 µF is the maximum derated capacitance that can be used for stability".
What happen when i use 100uF.
Thanks,
Hello,
Using output capacitor higher than mentioned in the Recommended operating table conditions can lead to unstable operation on the LDO output.
There is very high possibility of oscillation on LDO output, when 100uF capacitor is used.
Regards,
Rohit Phogat