This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65950 Tri-state PCM & I2S Pins

Other Parts Discussed in Thread: TPS65950, OMAP3530

Hello,

 

Can anyone confirm the following registers/bits on the TPS65950 programmed via I2C successfully allow the 4 pins of each port to coexist with another device?  I am looking to share McBSP Channels 2 & 3 from an OMAP3530 between a TPS65950 and another IC.    The pins on the off-module device can be tri-stated already, so there is no conflict there.  The description on some of the other registers indicates that the Bluetooth/voice/audio interfaces are switched off, but is unclear if the I/Os are now floating.  If this is possible, then I think just CODEEPDZ would cause the desired tri-state, but the rest are there for thoroughness.

 

Register Bit Value Description
CODEC_MODE CODECPDZ 0 Codec Powered Off
AUDIO_IF AIF_TRI_EN 1 High Impedance
AUDIO_IF AIF_EN 0 Off mode DIN/DOUT/SYN/CLK = L
VOICE_IF VIF_DIN_EN 0 Off mode vdr = L
VOICE_IF VIF_DOUT_EN 0 Off mode pcm_vdx = L
VOICE_IF VIF_TRI_EN 1 High Impedance
VOICE_IF VIF_EN 0 Mode VDR and PCM_VDX = L
BT_IF BT_DIN_EN 0 Off mode BTDIN = L
BT_IF BT_DOUT_EN 0 Off mode BT_PCM_VDX = L
BT_IF BT_TRI_EN 1 High Impedance
BT_IF BT_EN 0 Mode BTDIN/BTDOUT = L)

 

Thank-you.