Hi team,
In the process of using 100A charging and discharge, charging 100A to full power, stopping 100A for 30 seconds, found that there was a discharge MOS smoke, and it burst. However, the discharge MOS does not have a short circuit, but the charging MOS test is short -circuit. MOS charging and MOS discharge each with 15. It should be able to support nearly 200A current. May I know is the MOS opened too slowly? How to adjust the circuit?
Best regars,
Annie Liu