This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Full charge capacity and remaining capacity

Part Number: BQ40Z80
Other Parts Discussed in Thread: GPCCHEM

Hi Team,

When the mass-produced battery was used in the product, it was found that the fully charged capacity and the remaining capacity became 0. There is also a relative rate of change, the battery display is always 100%. Customer would like to know what causes the data to jump?

     

Best regards,

Annie Liu

  • Hello Annie,

    There are many reasons for FCC to report 0mAh. Can you share the .gg file and the log where this occurs? Did they perform a learning cycle and find the correct Chem ID using GPCCHEM?

    Sincerely,

    Wyatt Keller

  • Hi Wyatt Keller,

    20240108-1.log

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    Tue Jan 09 01:28:17 CST 2024
    Device Name = bq40z80
    Firmware Version = V0_04_BLD0005
    Design Capacity = 2700
    Design Voltage = 19200
    Specification Info = 0x0031
    Manufacturer Date = 2023-4-28
    Serial Number = 0x0001
    Manufacturer Name = CTECHI
    Device Name = GT500-22016-Bms-A2
    Device Chemistry = LFP
    Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,CellVolt5,CellVolt6,CellVolt7,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellCurr5,CellCurr6,CellCurr7,CellPower1,CellPower2,CellPower3,CellPower4,CellPower5,CellPower6,CellPower7,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,RaScale5,RaScale6,RaScale7,CompRes1,CompRes2,CompRes3,CompRes4,CompRes5,CompRes6,CompRes7,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,CellGrid5,CellGrid6,CellGrid7,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0_5,DOD0_6,DOD0_7,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,DODEOC_5,DODEOC_6,DODEOC_7,QMax1,QMax2,QMax3,QMax4,QMax5,QMax6,QMax7,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxDOD0_5,QMaxDOD0_6,QMaxDOD0_7,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,RawDOD_5,RawDOD_6,RawDOD_7,CBTime1,CBTime2,CBTime3,CBTime4,CBTime5,CBTime6,CBTime7,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBDOD_5,CBDOD_6,CBDOD_7,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus
    1,2024-01-09 01:28:21,4.004,0x0187,270,10,0x6001,0,65535,65535,1,18.6,20792,1510,1510,1,98,88,2356,2427,65535,65535,4,4004,21600,0x0080,6,-20578,-10408,-10800,-5400,95,0x0187,0x0000,0x04,0x0004,0x10,0x0D18,0x00B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3481,3461,3460,3452,3457,3486,0,20733,20873,1510,1510,1510,1511,1510,1510,0,526,523,522,522,522,526,0,3140,3136,30.9,24.2,18.5,-273.2,-273.2,18.5,24.2,18.5,2356,4457,2427,4591,2593,2447,4599,0,0,2518,4734,18.5,13.4,1000,1000,1000,1000,1000,1000,0,0,102,0,0,0,0,0,11,14,13,12,13,13,13,13,0,5651,0,0,0,0,0,0,0,71,135,47,0,0,0,0,0,0,0,2665,2717,2676,2671,2679,2683,0,0,0,0,0,0,0,0,71,47,10.0,18000,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,16384,2557,4778,1272,SUCCESS
    2,2024-01-09 01:28:25,8.012,0x0187,270,10,0x6001,0,65535,65535,1,18.6,20800,1510,1510,1,98,88,2358,2427,65535,65535,3,4004,21600,0x0080,6,-20579,-10409,-10800,-5400,95,0x0187,0x0000,0x04,0x0004,0x10,0x0D18,0x00B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3482,3462,3462,3452,3459,3488,0,20740,20881,1509,1510,1511,1510,1511,1509,0,525,523,523,521,523,526,0,3141,3137,30.5,24.3,18.6,-273.2,-273.2,18.6,24.3,18.6,2358,4460,2427,4591,2595,2448,4601,0,0,2518,4734,18.5,13.4,1000,1000,1000,1000,1000,1000,0,0,102,0,0,0,0,0,11,14,13,12,13,13,13,13,0,5655,0,0,0,0,0,0,0,70,133,47,0,0,0,0,0,0,0,2665,2717,2676,2671,2679,2683,0,0,0,0,0,0,0,0,70,47,10.0,18000,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,16384,2557,4778,1230,SUCCESS
    3,2024-01-09 01:28:29,12.015,0x0187,270,10,0x6001,0,65535,65535,1,18.6,20808,1510,1510,1,98,88,2359,2427,65535,65535,3,4004,21600,0x0080,6,-20579,-10409,-10800,-5400,95,0x0187,0x0000,0x04,0x0004,0x10,0x0D18,0x00B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3483,3464,3463,3453,3459,3490,0,20748,20890,1510,1510,1511,1510,1510,1509,0,526,523,523,521,522,527,0,3143,3138,30.8,24.2,18.6,-273.2,-273.2,18.6,24.2,18.6,2360,4464,2427,4591,2597,2450,4605,0,0,2518,4734,18.5,13.4,1000,1000,1000,1000,1000,1000,0,0,102,0,0,0,0,0,11,14,13,12,13,13,13,13,0,5659,0,0,0,0,0,0,0,68,129,47,0,0,0,0,0,0,0,2665,2717,2676,2671,2679,2683,0,0,0,0,0,0,0,0,68,47,10.0,18000,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,16384,2557,4778,1261,SUCCESS
    4,2024-01-09 01:28:33,16.020,0x0187,270,10,0x6001,0,65535,65535,1,18.6,20816,1510,1510,1,98,88,2361,2427,65535,65535,3,4004,21600,0x0080,6,-20581,-10409,-10800,-5400,95,0x0187,0x0000,0x04,0x0004,0x10,0x0D18,0x00B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3485,3466,3465,3454,3461,3491,0,20757,20901,1510,1510,1511,1510,1511,1509,0,526,523,524,522,523,527,0,3144,3139,30.8,24.2,18.6,-273.2,-273.2,18.5,24.2,18.5,2361,4467,2427,4591,2598,2452,4609,0,0,2518,4734,18.5,13.4,1000,1000,1000,1000,1000,1000,0,0,102,0,0,0,0,0,11,14,13,12,13,13,13,13,0,5664,0,0,0,0,0,0,0,66,125,47,0,0,0,0,0,0,0,2665,2717,2676,2671,2679,2683,0,0,0,0,0,0,0,0,66,47,10.0,18000,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,16384,2557,4778,1316,SUCCESS
    5,2024-01-09 01:28:37,20.025,0x0187,270,10,0x6001,0,65535,65535,1,18.6,20826,1509,1510,1,98,88,2363,2427,65535,65535,3,4004,21600,0x0080,6,-20582,-10410,-10800,-5400,95,0x0187,0x0000,0x04,0x0004,0x10,0x0D18,0x00B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3486,3467,3467,3455,3463,3493,0,20767,20907,1510,1510,1510,1511,1510,1509,0,526,524,524,522,523,527,0,3145,3140,30.6,24.2,18.6,-273.2,-273.2,18.6,24.2,18.6,2363,4470,2427,4591,2600,2453,4611,0,0,2518,4734,18.5,13.4,1000,1000,1000,1000,1000,1000,0,0,102,0,0,0,0,0,11,14,13,12,13,13,13,13,0,5667,0,0,0,0,0,0,0,65,123,47,0,0,0,0,0,0,0,2665,2717,2676,2671,2679,2683,0,0,0,0,0,0,0,0,65,47,10.0,18000,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,16384,2557,4778,1249,SUCCESS
    6,2024-01-09 01:28:41,24.040,0x0187,270,10,0x6001,0,65535,65535,1,18.6,20835,1510,1510,1,98,88,2364,2427,65535,65535,3,4004,21600,0x0080,6,-20581,-10409,-10800,-5400,95,0x0187,0x0000,0x04,0x0004,0x10,0x0D18,0x00B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3487,3470,3468,3456,3464,3495,0,20775,20919,1510,1510,1511,1510,1509,1510,0,527,524,524,522,523,528,0,3147,3142,30.9,24.2,18.6,-273.2,-273.2,18.6,24.2,18.6,2365,4473,2427,4591,2602,2455,4615,0,0,2518,4734,18.5,13.4,1000,1000,1000,1000,1000,1000,0,0,102,0,0,0,0,0,11,14,13,12,13,13,13,13,0,5671,0,0,0,0,0,0,0,63,119,47,0,0,0,0,0,0,0,2665,2717,2676,2671,2679,2683,0,0,0,0,0,0,0,0,63,47,10.0,18000,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,16384,2557,4778,1252,SUCCESS
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    7801.20240108-1.log

    Regards,

    Annie

  • Hello Annie,

    All the logs shared do not share the behavior described in the original post, also the .gg file is not attached.

    Sincerely,

    Wyatt Keller