This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSEMTHR24EVM-081: POE GUI Can not connect

Part Number: PSEMTHR24EVM-081
Other Parts Discussed in Thread: USB2ANY

您好,目前有使用到你們的PSEMTHR24EVM-081的板子,搭配PSIL083A和PSIL082A,並透過POE技術供電給PD端,然而當我想使用USB2ANY ADATER連結PC與我的電腦時,發生異常,異常狀況如下,想詢問有甚麼解決方法嗎? 

  • Hi Pojui,

    Thanks for reaching out.

    PSE expert is on holiday vacation. Please expert a delayed replay and sorry for the inconvenience.

    Best regards,

    Diang

  • Hi Pojui,

    It seems the MSP430 device on PSIL082 is not up to date with the latest FW version of the BSL code. 

    You may access the BSL code from your mysecure resources. The folder that should be used for this is FirmPSE folder. Using this folder, please navigate to PSE_BSL_Firmware_v03.exe. This is the executible that will download the BSL FW code. Once the BSL FW is downloaded. Please follow the steps in the User's Guide here for how to flash the BSL code.

    Once the BSL is correctly flashed, you may use the USB2ANY connector in order to connect to the device. 

    Regards,

    Brandon