Other Parts Discussed in Thread: LMR51610
I'm using the LMR38020FSDDAR variant of the part. When using the equations in the specification to select an inductor, the size of the inductor isn't matching the WEBENCH value.
The design is using the following design parameters:
Vin: 4.2V - 6V
Vout: 3.3V @ 300mA, 50C
The switching frequency was self-selected by WEBENCH as 406kHz
Custom output options:
UVLO enabled
Transient Vout change: 3%
Transient response current step: 0.1A
Max Vout ripple: 1%
Output caps: All ceramic
Power Good resistor: connected to Vout
Cff design: enabled
The recommend design shows Cboot=0.1uF, Cff=68pF, a 10uH inductor and for my companion output capacitors, I've selected an alternate custom group of 4 Murata 22uF 10%, 25V ceramic 1210 caps, 2mOhm ESR each. Based upon the inductor recommended value, I'm intending on using a Bourns SRP5050FA-100M1 (10uH, 20%, DCR=43mOhm (max), Isat=6.5A). I created a spreadsheet for the equations shown in the specification to allow easier Rfbb and Rfbt selection and optimum inductor choice using equation (10). My actual resistors are Rfbb=17.4K and Rfbt=40.2K which yields Vout=3.310V.
Lower down the WebBench page, the operating values were also adjusted to Vin=5.0V and Iout stayed as 0.3A.
The discrepancy I'm seeing has to do with the inductor calculation from equation (10). When using the same fsw=406kHz, Iout=0.3A, the inductor is shown to be 23uH instead of the 10uH from WEBENCH.
I have the following questions:
1. Why the difference in the values of the inductor?
2. Does the calculation in WEBENCH or the equations change if the inductor is shielded?
3. The specification describes AUTO mode and Forced PWM mode. Are these modes select-able or does the suffix of the part determine which mode is used?
4. Does the inductor selection through equation (10) assume Auto or FPWM mode, or does it not matter?
5. From my design, would it have been better to design around the LMR38020SDDAR instead of the LMR38020FSDDAR?
I'm attaching the downloaded Excel operating parameters from WEBENCH if it is allowed.